Jak vám dnes můžeme pomoci?

Is Resi9 MP IP41?

Issue:
I need an IP41 Resi9 MP enclosure.

Product Line:
Resi9 MP

Resolution:
Yes, thanks to an additional kit resi9 MP can reach IP41 in both installation, flush and surface.

Notes:
The commercial reference of the IP41 additional kit is MIP99034.
Instruction Sheet BBV48376