Jak vám dnes můžeme pomoci?

What is the drive fan number for the ATV660C16T4N2 drive?

Issue:
Need to replace the drive fan in a ATV660 drive.

Product Line:
ATV660

Environment:
ATV660C16T4N2

Cause:
Drive fan needs replaced.

Resolution:
VX5VPM001 is the heatsink 48vdc fan

VX5VPM003 is the enclosure Door 48vdc fan