Jak vám dnes můžeme pomoci?

Where in the menus is the ATV320 analog input image?

Issue:

It appears that the AI1C, AI2C and AI3C images for the input are not available.

Product Line:

ATV320

Environment:

All models

Cause:

Keypad monitoring of analog input signal

Resolution:

Navigating to the Monitoring menu, IO Map, Analog Inputs image to show the input V or mA signal value is only accessible with a connected graphic display keypad. The integral keypad will show the analog input assignment, but not the input value. Options for a graphic display keypad include VW3A1101 and VW3A1111.