Is the EVlink Pro AC compliant with Historical TIC and Standard TIC ?
The module card is the same if you use Historical TIC or Standard TIC.
The reference of the accessory card to be used is EVA1MTH (TIC interface) and Installation guide GEX2219201.
The configuration is done using eSetup,(see below).



The reference of the accessory card to be used is EVA1MTH (TIC interface) and Installation guide GEX2219201.
The configuration is done using eSetup,(see below).
Publikováno pro: Schneider Electric Česká republika