Jak vám dnes můžeme pomoci?

Why are the OPC UA client values not updating when using the UA_ReadList function block?

Changing the value type of the OPC UA client may prevent the client values from updating.

Performing the following steps may resolve the issue:
  1. Export the project as a .ZEF file
  2. Import the .ZEF file
  3. Run a Rebuild All project
  4. Download Project to controller