Jak vám dnes můžeme pomoci?

How do I assign Freewheel Stop to a Logic Input on AT320 drive?

Issue:
Programming Freewheel stop assignment to a Digital Input on ATV320.

Product Line:
Altivar 320, ATV320

Environment:
All models and serial numbers

Cause:
None

Resolution:
Goto DRI- > CONF > FULL > FUN- > STT- nSt and assign a logic input (LIx) as desired.
The stop is activated when the input changes to 0.
If the input returns to state 1 and the run command is still active, the motor will only restart if [2/3 wire control] (tCC) is set to [2 wire] (2C) and if [2 wire type] (tCt) is set to [Level] (LEL) or [Fwd priority] (PFO).
If not, a new run command must be sent.
Note: This function cannot be used with certain other functions. Follow the instructions in the Programming manual.