Jak vám dnes můžeme pomoci?

What is the Role and where can I find the certificates installed with CEV15.3?

Context
The Control Expert V15.3 certificates, which are created during installation, are in the LM store => Personal, here :
Certificates

To access it, you must launch certlm.msc via CMD. Control Expert V15.3 installs two self-signed certificates:
They are used to launch TM (Toplology Manager), to enable a PLC connection via HTTPS, and also to use the Security Service's Remote Security Database.
When launching TM (Topology Manager), at the beginning the SecurityServiceV1.0_WTFRLVSE182093L certificate is used and after ControlExpertV15.3_WTFRLVSE182093L. Regarding the PLC connection via HTTPS, the ControlExpertV15.3_WTFRLVSE182093L certificate is used. Finally, for the use of Security Service's Remote Security Database, SecurityServiceV1.0_WTFRLVSE182093L is used.

Product Line
PLC Quantum, PLC Premium, PLC M340 et PLC M580

Environment
Windows 10 64-bit (version 21H1 or newer), Windows 10 64-bit Enterprise 2019 LTSC (version 1809), Windows Server 2019 (standard 1809 version), Windows 11 64-bit (version 21H1 or newer), Windows Server 2022 (version 21H1 or newer), Control_Expert_V15.3