Jak vám dnes můžeme pomoci?

What size MicroSD card can the HDPM6000 support?

Issue
What size MicroSD card can the HDPM6000 support?

Product Line
HDPM6000

Resolution
32GB is the maximum size of MicroSD card that the HDPM6000 can support.

Additionally, 8GB is the minimum size of MicroSD card that the HDPM6000 can support.