Programming a digital input for fault reset on an ATS480 softstart?
Navigate under Menu 4 inputs/outputs menu.
Find Di3 and DI4 assignments.
The preferred input can be programmed as fault reset (LIRSF). This will allow the device to clear a detected error with the toggle of a contact made between DI3 or DI4 to 24V terminal.