Jak vám dnes můžeme pomoci?

How do I connect to the Edge I/O Network Interface Module via USB connection

Issue:

USB connection to the Edge I/O NIM


Product Line:

Edge I/O


Resolution:

The USB Port connection is suitable for short-duration connections for the express purposes of configuration, maintenance, and troubleshooting. It is not intended as a long-standing connection for other purposes. Further, the network interface module may only be connected to a PC.

Note: The communication cable should be connected to the PC first to help minimize the possibility of electrostatic discharge affecting the network interface module

image1

To connect the network interface module to the PC, do the following:

image2

You must configure a virtual Ethernet Link on your USB port, before you can access the network interface module through USB.

To configure a virtual Ethernet Link, configure an Ethernet interface of the USB-RNDIS by following the steps below:

image3