Issue:
Wondering if the Altistart Soft Starts are SEMIF47 Compliant?
Product Line:
Altistart
Environment:
All
Cause:
SEMIF47 compliant
Resolution:
The Altistart soft starts are not SEMIF47 Compliant, as they do not have enough stored capacity to ride through a power dip or sag.
 
Veröffentlicht für: Schneider Electric Deutschland