How to get SCADAPack E Series Dump Files?
To get dump files follow the below steps:
1. While connecting to SCADAPack E >Open Remote Command-Line from Transfer Menu
2. Write this command “dir” in the Command-Line window
3. From Transfer Menu select “Read File”
4. A new pop-up window open copy the name of the dump file from Virtual Terminal Command, paste it in the File name as below image, and press save.
5. The Dumb file will be created in the previously selected directory with the same name.
Udgivet til:Schneider Electric Danmark