¿Cómo podemos ayudarle hoy?

Can SoMove Software be used to monitor multiple drives over a Modbus network?

Issue:
Can SoMove Software be used to monitor multiple drives over a Modbus network?

Product Line:
Altivar Process Drive

Environment:
All models and serial numbers

Cause:
Wiring / Programming

Resolution:
You can use the resident Modbus RTU on the drive so no Gateway is required.  You would configure each drive with a Modbus Network address.  Cable used to daisychain  (VW3A8306TF03 or ..F10) via Modbus.
The cable is F03=.3 M or 1ft, or 10= 1.0M or 3ft.   Set the Scan up as Multipoint, and have to setup the range of registers.