Hae usein kysyttyjä kysymyksiä
When the power of Altivar 32 drive is recycled, then the parameter value has not been saved to the Altivar 32 drive, which is change by communication.
When a value is modified by the communication (Modbus, CANopen, or other communication board), the parameter is only write
in drive RAM.So when the drive is Power OFF/ON, the value is lost and the parameters revert to the last saved value in EEPROM.
in drive RAM.So when the drive is Power OFF/ON, the value is lost and the parameters revert to the last saved value in EEPROM.
To write a parameter in Drive EEPROM, it is necessary to write CMI (logic address 8504) bit 1.
Refer to attached file for detail.
Refer to attached file for detail.
Julkaistu:Schneider Electric Suomi
Liitteet
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: