Hae usein kysyttyjä kysymyksiä
Which Magelis HMIs can support with XBTL1001 and which Magelis HMIs do I require XBTL1003M to support?
Issue
Which Magelis HMIs can support with XBTL1001 and which Magelis HMIs do I require XBTL1003M to support?
Product Line
Magelis XBT-L
Environment
XBTL1003M
Resolution
XBTL1001M (the XBTL1000 light software package) only supports the XBTN, XBTH, XBTE, XBTP, XBTHM and XBTPM Alphanumeric Magelis terminals.
XBTL1003M (the XBTL1000 full software package supports the XBTN, XBTH, XBTE, XBTP, XBTHM and XBTPM Alphanumeric Magelis terminals as well as the XBTF Graphical Magelis terminals.
Julkaistu:Schneider Electric Suomi
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: