Hae usein kysyttyjä kysymyksiä
Which Modbus function codes are supported by the TSXETG100 Modbus to Ethernet bridge?
Issue
Which Modbus function codes are supported by the TSXETG100 Mobdus to Ethernet bridge?
Product Line
ConneXium - Ethernet
Environment
TSXETG100
Resolution
TheTSXETG100 Modbus to Ethernet bridge supports all Modbus function codes. The bridge does not filter any function codes. The bridge takes the data from an Ethernet packet and sends it serially or takes the serial data and places it an Ethernet packet.
Julkaistu:Schneider Electric Suomi
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: