Hae usein kysyttyjä kysymyksiä
PM600 Series Available Onboard Alarms
Issue
What onboard Alarms are available for PM600 Series meters?
Product Line
PM600
PM620
PM650
Environment
Onboard Alarming Capability
Resolution
There are no onboard alarms available for the PM600 and PM620 meters, however, PC Based alarming can be created via software.
The PM650 does have onboard alarming capabilities (30 alarm conditions). See page 66 of the PM600 Series User Guide
Julkaistu:Schneider Electric Suomi
Liitteet
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: