Tuotemerkkimme

Impact-Company-Logo-English Black-01-177x54

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
The ATV58 option card has an IC labeled POTAIN, What does POTAIN refer to?

Issue:
What does " POTAIN " refer to?

Product Line:
Altivar Machines, Altivar 58

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
It’s a specific card for the crane builder POTAIN Crane (see label on the microchip).
For technical support on this board, contact POTAIN Crane.