This class specifies the minimum value of the knee point voltage (Vk) of the CT. It also imposes a maximum value of CT secondary winding resistance (Rct). Sometimes, it specifies the maximum value of the magnetizing current (Io) at knee point voltage.