Hae usein kysyttyjä kysymyksiä
Can I use the service port on the M580 HSBY processor for SCADA traffic while servicing ERIO ?
Not recommended. Please consider using an NOC module. The service port does not support Rapid Spanning Tree Protocol and as a result the connection of each of these ports to a SCADA can result in an excessive amount of broadcast or ARP traffic.
We recommend using the NOC option module for SCADA in HSBY applications.
We recommend using the NOC option module for SCADA in HSBY applications.
Julkaistu:Schneider Electric Suomi
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: