{}

Tuotemerkkimme

Impact-Company-Logo-English Black-01-177x54

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.

Hae usein kysyttyjä kysymyksiä

What is the minimum distance between the Vigirex rectangular sensor and the following bending of the busbar?

Depending on the size of the sensor, the following minimum distances must be respected:
- 280 x 115 mm sensor -> the distance between the sensor and the busbar bending must be equal to, or higher than 25cm.
- 470 x 160 mm sensor -> the distance between the sensor and the busbar bending must be equal to, or higher than 30cm.

Schneider Electric Suomi

Lue lisää
Tuotesarja:
Vigirex RH10A-RH240-RH248-RH320VigiPacTVigirex Ground-fault Relay System
Lue lisää
Tuotesarja:
Vigirex RH10A-RH240-RH248-RH320VigiPacTVigirex Ground-fault Relay System