Tuotemerkkimme

Impact-Company-Logo-English Black-01-177x54

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
Exception response (4) in Power Monitoring Expert system event log with PM5560 and PM5300 series

Issue
User is seeing multiple events in the system log of Power Monitoring Expert "Exception response (4)" referencing PM5560 or PM5300 series devices.

Product
Power Monitoring Expert 8.2

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment
Management Console

Cause
When PME is trying to read a data log record from the device it is receiving an exception response. PME driver then makes an entry in the System Log and moves on to read the next record. These entries in the System Log are meant for diagnostics purpose so that we know why PME skipped reading a record

Resolution
Upgrade the firmware of the PM5560 or PM5300 series meter, see FA320492