Issue
Information about the 3 input phases does not appear on the PowerView display.
Product Line
Single Phase Symmetra
Environment
SYMSTRF3I with PowerView firmware below revision N.
Cause
The firmware on the PowerView must be at revision N or later for this information to be displayed. To check your firmware:
To check the firmware revision of the PowerView follow these steps:
1. Press any key to go to Menu screen
2. Scroll to Display menu and press enter
3. Scroll down to Information and press enter
4. Firmware is indicated in bottom right corner as FW=N4a (example only)
Resolution
If PowerView part no. AP9215 is in use, the firmware cannot be upgraded. If PowerView part no. AP215RM is in use, the firmware can be upgraded by downloading the latest firmware file and following knowledge base article FA156046.
פורסם עבור:שניידר אלקטריק ישראל