המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ProWORX 32 Server limitations

Issue
ProWORX 32 Server limitations

Product Line
ProWORX 32...All versions

Environment
Windows 7

Resolution

The following limitations have been found on the ProWORX 32 server.

  • If the server is being used for communicating to the PLC:
The limit is 3 for connecting to the PLC via the server and 5-8 users for
connecting to the server for puts and gets at the same time that the clients
are connected to the PLC via the server.
  • If the server is used only for project storage and retrieval (the server is not used for
communicating to the PLC):

No limitations on number of users simultaneously connected with
either Modbus Plus or TCP/IP other than what is allowed for the server PC's
Microsoft Windows operating system's TCP/IP connections and the Modbus Plus
Adapter card.
  • Maximum number of users configured on the server:
  • No limitations.
  • Maximum number of projects stored on the server.

No limitations other than the hard drive free space capacity.