Issue
How many devices does each port of the EGX product line support?
Product Line
EGX100/200/300/400
Resolution
Each serial port can communicate with 32 devices without repeaters. The EGX100/300 products have a single serial port, while the EGX200/400 have two serial ports and hence can communicate with up to 64 devices.
פורסם עבור:שניידר אלקטריק ישראל