המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Object Error in ENM
Issue
In ENM while selecting Email from the Relay Name drop down list, an object error message opened:



Product Line
Event Notification Module 7 (ENM)

Environment
Web Browser
Internet Explorer
Windows Server 2008 R2

Cause
Windows updates were applied and IE8 (Internet Explorer 8)  was upgraded to IE11.
ENM 7 only supports IE8 in compatibility mode.

Resolution
Internet Explorer 11 was uninstalled and the browser went to the default IE8.  This resolved the problem.