{}

המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
Downloading and updating the firmware of PM5XXX using DLF-3000 3.3 v 2
Issue
Need to update PM5XXX firmware.

Product Line
PM5XXX
DLF-3000

Environment
Firmware Upgrade

Cause
Firmware related issue.

Resolution
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.

*Warning: Be sure all other software, is not connected to the meter.*

Use the following link to download the DLF-3000 software:

DLF-3000 Download

The attached tutorial will walk you through how to update the firmware of a PM5XXX meter using DLF-3000 software and serial or ethernet connection.

שניידר אלקטריק ישראל

קבצים מצורפים
PM5xxx - FW Update through DLF3000 - Method.pdf [1.84 MB]