שאלות נפוצות
Safety limit switches XCS_UL certificate of the XCSDMP, XCSDMC and XCSDMR magnetic switches
Please find attached the UL certificate n°NKCR.E164353 concerning Sensors auxiliary devices. In this certificate, the magnetic switches are classified as proximity switches. Only the ref. of the switch sub-assemblies are indicated, like indicated on the switch marking.
Proximity switches Model(s) XCS, followed by ZC, ZP or ZR, followed by 5 or 7, followed by 0 or 9, followed by 0 or 1, followed by 1, 2 or 5, may be followed by 0, may be followed by LxxM8 or LxxM12.
Proximity switches Model(s) XCS, followed by ZC, ZP or ZR, followed by 5 or 7, followed by 0 or 9, followed by 0 or 1, followed by 1, 2 or 5, may be followed by 0, may be followed by LxxM8 or LxxM12.
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד