המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Unity help incorrectly states that the outputs on the BMXDDI1602 are isolated.
Issue
Unity help incorrectly states that the outputs on the BMXDDI1602 are isolated.

Product Line
x80 Modules, EcoStruxure Control Expert (formerly known as Unity Pro)

Environment
Windows 7 Professional, Unity Pro 8.1, BMXDDI1602.

Resolution
  • Unity help incorrectly shows that the outputs on the BMXDDI1602 are isolated.



  • The wiring diagram from the user manual correctly shows the outputs as not being isolated.