שאלות נפוצות
Rope pull switches XY2C - Where are indicated the commercial ref. and the production date on the XY2CH rope pull switch
On the XY2CH E.stop rope pull switches, the commercial reference and the manufacture date, or date code, are indicated in the product label, sticked on the largest side of the switch. The production date is indicated like that : Year - Week. Please have a look at the attached label example. In the past the commercial reference and the production date were marked on a little label separated from the main label
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד