Issue:
What are the difference between the HMIG3U versus HMIG5U?
Product Line:
HMIG3U, HMIG5U
Resolution:
The HMIG3U is a Magelis operating in a proprietary OS with Runtime. Whereas, the HMIG5U is running Windows 7 Embedded operating system with PC base Runtime.
What are the difference between the HMIG3U versus HMIG5U?
Product Line:
HMIG3U, HMIG5U
Resolution:
The HMIG3U is a Magelis operating in a proprietary OS with Runtime. Whereas, the HMIG5U is running Windows 7 Embedded operating system with PC base Runtime.
פורסם עבור: שניידר אלקטריק ישראל