המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is an OSF (over voltage) fault on an ATS22 soft start?

Article available in these languages: Czech

Issue:
What are the steps to troubleshoot an OSF [Over Supply Fault] on an ATS22 soft start?

Product Line:
ALTISTART 22, ATS22

Environment:
All

Cause:
Over voltage condition

Resolution:
Overvoltage fault.
Check ULN parameter under CONF menu.  This should match your line voltage.
Check the power supply circuit and voltage.  Reading will need to be balanced phase to phase on L1, L2, and L3 and match voltage spec for the softstart and motor.
Check OSD [Over voltage Threshold] and OST [Over voltage Time Delay] parameters in PRO menu for possible adjustments.