המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Do we have fuse on our PCB board in the base station, if customer wiring the wrong Voltage it will protect the base station. If we have, can you give me the picture to show which one is Fuse. And if the fuse was burned, how to change a new one. Because th
There are fuses in our base. It is not possible for the customer to change them. By the way you have to use a external protection as mentioned in the User Guide and User Manual.