שאלות נפוצות
Osisense XC - Where is the product reference indicated on the XCMD and XCMN limit switch series
The complete reference is indicated on the XCMN plastic miniature switch, not sold in sub-assemblies, on the side where the contact representation is. Have a look at the attached picture. For the XCMD metal miniature switches, sold with variable composition body + head + lever if necessary, the reference of each sub-assemblies is indicated on each part. See the attached pictures showing an example of ZCMD body and of ZCE10 head
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד