Issue:
What address can you read on the ATV61 and ATV71 drives to show the last fault using Ethernet TCP IP or Modbus?
Product Line:
ATV61 and ATV71
Environment:
All
Cause:
Wants to read current fault of the drive not the fault history.
Resolution:
LFT or last fault error in address 7121
What address can you read on the ATV61 and ATV71 drives to show the last fault using Ethernet TCP IP or Modbus?
Product Line:
ATV61 and ATV71
Environment:
All
Cause:
Wants to read current fault of the drive not the fault history.
Resolution:
LFT or last fault error in address 7121
LFT0[No Error] (nOF)
2[EEPROM Control] (EEF1)
3[Incorrect Configuration] (CFF)
4[Invalid Configuration] (CFI)
5[Modbus Com Interruption] (SLF1)
6[Internal Link Error] (ILF)
7[Fieldbus Com Interrupt] (CnF)
8[External Error] (EPF1)
9[Overcurrent] (OCF)
10[Precharge Capacitor] (CrF)
13[AI2 4-20mA loss] (LFF2)
15[Input Overheating] (IHF)
16[Drive Overheating] (OHF)
17[Motor Overload] (OLF)
18[DC Bus Overvoltage] (ObF)
19[Supply Mains Overvoltage] (OSF)
20[Single output phase loss] (OPF1)
21[Input phase loss] (PHF)
22[Supply Mains UnderV] (USF)
23[Motor short circuit] (SCF1)
24[Motor Overspeed] (SOF)
25[Autotuning Error] (tnF)
26[Internal Error 1] (InF1)
27[Internal Error 2] (InF2)
28[Internal Error 3] (InF3)
29[Internal Error 4] (InF4)
30[EEPROM Power] (EEF2)
32[Ground Short Circuit] (SCF3)
33[Output Phase Loss] (OPF2)
34[CANopen Com Interrupt] (COF)
37[Internal Error 7] (InF7)
38[Fieldbus Error] (EPF2)
40[Internal Error 8] (InF8)
42[PC Com Interruption] (SLF2)
45[HMI Com Interruption] (SLF3)
51[Internal Error 9] (InF9)
52[Internal Error 10] (InFA)
53[Internal Error 11] (InFb)
54[IGBT Overheating] (tJF)
55[IGBT Short Circuit] (SCF4)
56[Motor Short Circuit] (SCF5)
60[Internal Error 12] (InFC)
64[Input Contactor] (LCF)
68[Internal Error 6] (InF6)
69[Internal Error 14] (InFE)
71[AI3 4-20mA loss] (LFF3)
72[AI4 4-20mA loss] (LFF4)
73[Boards Compatibility] (HCF)
77[Conf Transfer Error] (CFI2)
79[AI5 4-20 mA loss] (LFF5)
99[Channel Switch Error] (CSF)
100[Process Underload] (ULF)
101[Process Overload] (OLC)
105[Angle error] (ASF)
106[AI1 4-20 mA loss] (LFF1)
107[Safety Function Error] (SAFF)
110[AI2 Th Detected Error] (tH2F)
111[AI2 Thermal Sensor Error] (t2CF)
112[AI3 Th Detected Error] (tH3F)
113[AI3 Thermal Sensor Error] (t3CF)
114[PumpCycle Start Error] (PCPF)
115[Out Pressure Low] (OPLF)
116[High Flow Error] (HFPF)
117[Inlet Pressure Error] (IPPF)
119[Pump Low Flow Error] (PLFF)
120[AI4 Th Detected Error] (tH4F)
121[AI4 Thermal Sensor Error] (t4CF)
122[AI5 Th Detected Error] (tH5F)
123[AI5 Thermal Sensor Error] (t5CF)
124[Anti Jam Error] (JAMF)
125[Out Pressure High] (OPHF)
126[Dry Run Error] (DRYF)
127[PID Feedback Error] (PFMF)
128[Program Loading Error] (PGLF)
129[Program Running Error] (PGrF)
142[Internal Error 16] (InFG)
143[Internal Error 17] (InFH)
144[Internal Error 0] (InF0)
146[Internal Error 13] (InFd)
148[Motor Stall Error] (StF)
פורסם עבור:שניידר אלקטריק ישראל