המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can historical data be transferred automatically from ION6 to Power Manager 1.3?
The historical data cannot be transferred automatically, but must be done manually which is a lengthy process.

This is done using SQL database.

It cannot be done using something like ETL as ETL is only to be used between Schneider Electric software.

Please see email explaining that the historical data must be transferred using SQL database.

If the historical data is needed a suggestion it to upgrade to the latest version PME, 8.2, as the historical data with be transferred automatically.