Issue:
When you navigate to Diagnostic Viewer > Service Diagnostics > Communication Server you see the tree state shows "BAD" as shown in the below screenshot.
Product Line:
Power Monitoring Expert 2020
Environment:
Diagnostic Viewer
Cause:
This is a bug with the PME Diagnostic Viewer. It is just a display issue and does not affect PME in any other way.
Resolution:
It will be addressed in PME 2020 CU1
פורסם עבור: שניידר אלקטריק ישראל