What can be the root cause of SAFF fault with SAF1=1 on ATV32 or ATV320?
Issue: SAFF fault on ATV32 or ATV320 drives Product Line: ATV32 or ATV320 Environment: SAFF fault Cause: n/a Resolution: The SAFF could have a lot of root causes. Here are some examples in the...