¿Cómo podemos ayudarte hoy?

Can the 8910DP** or 8910DPA** definite purpose contactors be field converted to 8911DS or 8911DPS definite purpose starters?

Issue:
Are the 8910DP** or 8910DPA** definite purpose contactors be converted to 8911DS or 8911DPS definite purpose starters?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8903 Type DP, DPA
​
Resolution:
There is no direct mount overload relays available for this conversion. However, if there is enough enclosure space this can be accomplished by the use of a separate mount overload relay.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango:
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
  • Obtén un presupuesto
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
  • Términos y condiciones
  • Change your cookie settings
  • Centro de Preferencias