¿Cómo podemos ayudarte hoy?

Can the Powerpact P frame breakers be used in existing old style I-Line panelboards?

Issue:
Powerpact P frame used in older I-Line panelboards?

Product Line:
?I-Line Panelboards.

Environment:
Products sold in North America

Resolution:
Schneider Electric/Square D evaluated the construction of existing I-Line Panelboards and Switchboards and previously manufactured and installed Panelboards and Switchboards and has confirmed they are the same in basic construction. Further evaluation shows the use of I-Line circuit breakers with the prefix ``H``, ``J``, ``MG``, ``MJ``, ``P`` and ``R`` frame , to be acceptable for installation and use within these existing Panelboards and Switchboards previously installed in the field. Care should be taken that voltage and AIC ratings match, are confirmed and compatible between the circuit breaker and the electrical equipment.