{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
How to Configure a Modbus-Advanced Generic Direct Outstation in ClearSCADA?
The following article describes the steps necessary to configure a Modbus-Advanced Generic Direct Outstation over TCP/IP Connection in ClearSCADA as follows:

1- Make sure that Modbus-Advanced Driver is installed, check the below link of how to install a driver in ClearSCADA
https://www.se.com/ww/en/faqs/FA382995/

2- Create a Modbus-Advanced Direct Channel- right-click where you want to create the channel, select Modbus-Advanced and select Direct Channel.




3- Configure the Direct Channel as follows:







4- Create Modbus-Advanced Direct Outstation Set- right-click where you want to create the Outstation set, select Modbus-Advanced and select Direct Outstation Set.




5- Configure the Direct Outstation Set as follows:





6- Create Modbus-Advanced Generic Direct Outstation- right-click where you want to create the Outstation, select Modbus-Advanced, select Generic and select Direct Outstation.




7- Configure the Direct Outstation as follows:








Note: Check the Windows firewall settings to make sure that the windows firewall does not block the connection.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: