¿Cómo podemos ayudarte hoy?

How do I select an appropriate wall mounting bracket for a low voltage general purpose Transformer? Please provide an example with a EXN75T3H.

Issue:
Wall Mounting Transformer

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Ventilated Transformers require Wall Mounting Brackets

Resolution:


If the Transformer is listed in the Digest, you can look up the enclosure number and the Wall Mounting Bracket from the appropriate page.

Example:  EXN75T3H -- is shown in enclosure 20M.  The Digest indicates a 7400WMB18M19M20M Wall Mounting Bracket