¿Cómo podemos ayudarte hoy?

Are all Low Voltage Dry Type Distribution Transformers tested before they leave the factory? If so, what are the standard routine commercial product tests done on each Transformer?

Issue:
ST-20 Standard for Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Transformer testing

Resolution:

Every SquareD/Schneider Electric Low Voltage Dry Type Distribution Transformer receives and must pass the following tests per NEMA ST-20 before it is allowed to leave the factory:

Visual
Polarity and Phase Relation
Ratio-tests
No-load Losses and excitation Current
Dielectric - Applied potential and Induced potential

As well, there are additional tests completed per NEMA ST-20 on first design of each transformer rating:

Impedance
Load Loss
Dielectric - Impulse
Audible Sound Level