¿Cómo podemos ayudarte hoy?

Do the Motor-Logic solid state overload relays use the same coil in the starter as starters that come with melting alloy or bi-metallic overload relays?

Issue:
Are the Motor-Logic solid state overload relays coil the same as starters that come with melting alloy or bi-metallic overload relays?

Product Line:
NEMA Contactors and Starters

Environment:
Class 9065 Motor Logic solid-state overload relays (SSOLRs)

Resolution:
Yes. A difference in overload relay does not affect the type of coil used in the starter.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: