¿Cómo podemos ayudarte hoy?

What is the Branch Circuit Power Meter with Ethernet communications module integrated (BCPME) Graphic User Interface (GUI) login credential?

Issue
BCPME GUI access denied while trying to configure the device web server for the first.

Product Line
Branch Circuit Power Meter with Ethernet communications module integrated (BCPME)

Environment
Installation and accessories

Cause
Username and password unknown

Resolution
The BCPME comes with a default IP address and subnet mask (192.168.1.24/255.255.255.0), this helps to setup the Laptop or PC with a static IP address and mask like (192.168.1.30/255.255.255.0), connect to the meter then configure it. See the user guide from pages 16-20 for procedure detail.
But to access the Graphic User Interface (GUI) you will require the Username and the Password. The username is “admin”, but the password is default alphanumeric, unique for each device, and can be found on the barcode label which is affixed to the metal enclosure of the product. You are recommended to change it after login the GUI. See user guide on page 32.

Find the link below for the BCMPE user guide, note that the pages may change if there is an update of the documentation.
  • BCPME_Z206856-0D
https://www.se.com/ww/en/download/document/Z206856/

Other important link: BCPME_Part_Number
https://www.se.com/us/en/faqs/FA233733/