¿Cómo podemos ayudarte hoy?

What are the VR Circuit Breaker Weight?

Issue:
Sometimes it is required to move the VR breakers to storage, maintenance, or commissioning, so, the customers need to know the VR Breakers' weights to be prepared with the adequate crane

Product Line:
MV Switchgear.

Environment:
Metal Clad, VR Circuit Breaker.

Cause:
Storage, maintenance, or commissioning.

Resolution:
BREAKER WEIGHT
5/15kV BREAKER RATINGWEIGHT
1200A, 25kA & 40kA380 lbs
2000A, 25kA & 40kA430 lbs
1200A, 50kA450 lbs
2000A, 50kA500 lbs
3000A, 4000A, 50kA700 lbs
1200A, 2000A, 3000A & 4000A 63kA800 lbs
27kV BREAKER RATINGWEIGHT
1200A, 16kA, 25kA & 40kA625 lbs
2000A, 16kA, 25kA & 40kA650 lbs
2750A, 16kA, 25kA & 40kA775 lbs