¿Cómo podemos ayudarte hoy?

What are the weights of the VR Circuit Breakers?

Issue:
Any job that involves moving the VR breaker, for instance; maintenance, storage, or commissioning, requires knowing its weight so that customers have the proper crane.

Product Line:
MV Switchgear.

Environment:
Metal Clad, VR Circuit Breaker.

Cause:
Maintenance / Commissioning.

Resolution:

BREAKER WEIGHT
15kV BREAKER RATINGWEIGHT
1200A, 25kA & 40kA380 lbs
2000A, 25kA & 40kA430 lbs
1200A, 50kA450 lbs
2000A, 50kA500 lbs
3000A, 4000A, 50kA700 lbs
1200A, 2000A, 3000A & 4000A 63kA800 lbs
27kV BREAKER RATINGWEIGHT
1200A, 16kA, 25kA & 40kA625 lbs
2000A, 16kA, 25kA & 40kA650 lbs
2750A, 16kA, 25kA & 40kA775 lbs