How many Current Transformers can be installed within MV Metal Clad Switchgear?
Issue:
Customers must be knowledgeable about the features and design of MV Metal Clad Switchgear to prevent errors and ensure it functions correctly to meet their requirements.
Product Line:
MV Switchgear.
Environment:
Metal Clad, VR Circuit Breaker.
Cause:
Maintenance and understanding the operation of the Metal Clad design.
Resolution:
Bushing-type, single- or multi-ratio Current Transformers can be mounted around either the top or bottom insulated tubes/Bell Assembly. A maximum of four Current Transformers can be mounted per phase, depending on the accuracy: For Standard Accuracy Current Transformers, two on the line side and two on the load side can be mounted. However, if High Accuracy Current Transformers are required, only one can be mounted on the line side and another on the load side.