¿Cómo podemos ayudarte hoy?

What are the weights of the Metal Clad Switchgear?

Issue:
Any job that involves moving the Metal Clad Switchgear, for instance; maintenance, storage, or commissioning, requires knowing its weight so that customers have the proper crane.

Product Line:
MV Switchgear.

Environment:
Metal Clad.

Cause:
Maintenance / Commissioning.

Resolution:

INDOOR
-  Switchgear Unit2100  lb.
-  Breaker – 1200A,  40KA380  lb.
-  Breaker – 1200A,  50KA430  lb.
-  Breaker – 2000A,  40KA450  lb.
-  Breaker – 2000A,  50KA500  lb.
-  Breaker – 3000A700  lb.
-  Breaker – 1200,2000,3000A, 63kA800  lb.
-  Drawout Unit (2) 15KV VT’s210  lb.
-  Drawout CPT 15KVA270  lb.
-  CPT Fixed Mounted  37.5KVA580  lb.
-  CPT Fixed Mounted  50KVA750  lb.
-  3 Arrester-Intermediate  15KV120  lb.
Average Switchgear Unit Weight2500  lb.
Average Switchgear Unit Weight, 63kA 2900  lb.

OUTDOOR NON-WALK-IN
NOTE: Outdoor weights are to be added to Indoor weights.
22.0 Wide Unit (Includes Base)595  lb.
36.0 Wide Unit (Includes Base)680  lb.
48.0 Wide Unit (Includes Base)1123  lb.
End Panel (Add 2)395  lb.

OUTDOOR WALK-IN
NOTE: Outdoor weights are to be added to Indoor weights.
22.0 Wide Unit (Includes Base)430  lb.
36.0 Wide Unit (Includes Base)530  lb.
38.0 Wide Unit (Includes Base780  lb.
48.0 Wide Unit (Includes Base)850  lb.
22.0 Wide Work Space430  lb.
36.0 Wide Work Space990  lb.
48.0 Wide Work Space1200  lb.
72.0 Wide Work Space1670  lb.

SINGLE WALK-IN AISLE
22.0 Wide Aisle340  lb.
36.0 Wide Aisle470  lb.
38.0 Wide Aisle490  lb.
48.0 Wide Aisle640  lb.

COMMON WALK-IN
22.0 Wide Aisle270  lb.
36.0 Wide Aisle370  lb.
48.0 Wide Aisle450  lb.
End Panel (Single or Common Aisle, Add 2)400  lb.
End Wall (Single or Common Aisle, Add 2)370  lb.