Merkene våre

Impact-Company-Logo-English Black-01-177x54

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
NetBotz 300-500 Series | SNMP MIB File
Issue:
SNMP MIB for NetBotz Version 2 and 3 Appliances

Product Line:
NetBotz 300-500 Series Version 3
v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)

Environment:
NetBotz v2/v3 (all versions)

Resolution:

The SNMP MIB for NetBotz Appliances can be downloaded from the NetBotz Appliance itself by accessing the following URL:

For version 3:
http://ip_address_of_appliance/netbotzv3.mib

For version 2:
http://ip_address_of_appliance/netbotzv2.mib